Part Number: MSP-EXP430G2ET
Other Parts Discussed in Thread: UNIFLASH
Using mspdebug under 64-bit Debian Linux 10, I am unable to connect to the MSP-EXP430G2ET Launchpad with mspdebug version 0.25. I have had no problems connecting to the older MSP-EXP430G2 Launchpad.
I read that the MSP-EXP430G2ET uses a different debug interface (eZ-FET). Trying "mspdebug ezfet" fails:
brad@bradsphenom:~$ mspdebug ezfet
MSPDebug version 0.25 - debugging tool for MSP430 MCUs
Copyright (C) 2009-2017 Daniel Beer <dlbeer@gmail.com>
This is free software; see the source for copying conditions. There is NO
warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.
Chip info database from MSP430.dll v3.3.1.4 Copyright (C) 2013 TI, Inc.
Reset communications...
Version: 2.11.0.1, HW: 0xaaadaaad
Reset firmware...
hal_proto_execute: HAL exception: 0xffff
hal_proto_execute: fid: 0x51
I also read that if 'ezfet' fails, it might be necessary to install libmsp430.so and use 'tilib'. This also fails:
brad@bradsphenom:~$ mspdebug tilib
MSPDebug version 0.25 - debugging tool for MSP430 MCUs
Copyright (C) 2009-2017 Daniel Beer <dlbeer@gmail.com>
This is free software; see the source for copying conditions. There is NO
warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.
Chip info database from MSP430.dll v3.3.1.4 Copyright (C) 2013 TI, Inc.
Using new (SLAC460L+) API
MSP430_GetNumberOfUsbIfs
No unused FET found.
On the off chance that it was a permissions issue, I tried the same with 'sudo', and got the same results both times.
I have read other posts on the e2e forum but have not seen a solution to this issue.