Part Number: MSP430F249
Tool/software: Code Composer Studio
Hello
I'm trying to use a temperature sensor(PCT2075) by MSP430
To get a temperature, I get a 2bytes from this sensor.
Howerver, I got just two same value. I think that it is MSByte.
I wrote a code from this link.
I'm using MSP430F249. so I modified a code from this link.
void i2c_read_multi(uint8_t slv_addr, uint8_t reg_addr, uint8_t l, uint8_t *arr)
{
uint8_t i;
while(UCB0STAT & UCBBUSY);
UCB0I2CSA = slv_addr; // set slave address
UCB0CTL1 |= UCTR | UCTXSTT; // transmitter mode and START condition.
while(UCB0CTL1 & UCTXSTT);
UCB0TXBUF = reg_addr;
while(!(UCB0CTL1 & UCTXSTT));
UCB0CTL1 &= ~UCTR; // receiver mode
UCB0CTL1 |= UCTXSTT; // START condition
while(UCB0CTL1 & UCTXSTT); // make sure start has been cleared
for (i = 0; i < l; i++) {
while(!(IFG2 & UCB0RXIFG));
if(i == l - 1){
UCB0CTL1 |= UCTXSTP; // STOP condition
}
arr[i] = UCB0RXBUF;
}
while(UCB0CTL1 & UCTXSTP);
}