Tool/software: WEBENCH® Design Tools
Hey,
I have begun having issues with the CapTIvate Design Studio. It used to open up just fine and I was able to use the application without any faults, but the application now does not show any window when I try and open up the application. All I see is the following now:
I am wondering if this is an issue seen before and if there is a fix. Is it possible that any hidden files this application uses could have been corrupted and therefore refused to show a window?
I have already tried uninstalled (via C:\ti\msp\CapTIvateDesignCenter_1.83.00.08\Uninstall_CapTIvateDesignCenter.exe) and re-installing the application, but that did not work. Here are the specifications of my system:
- Windows 10 x64
- Java Build 1.8.0_261-b12
- Design Studio Version 1.83.00.08
Has anyone seen this issue where the Design Studio will appear to open, but no GUI actually appears?
Thanks,
Dan