Part Number: MSP430G2553
Other Parts Discussed in Thread: PCF8574, , PCF8574A
Tool/software: Code Composer Studio
Hi, I am new at this. I am trying to interfacing 1602A LCD display with MSP430G2553 via PCF8574. When I run the code, nothing happens:
#include <msp430.h>
unsigned int *ptxData;
unsigned int count = 0;
// [0..3] -> power on, [4..5] -> function set, [6..7] -> display off, cursor off, blink off
// [8..9] -> clear screen, [10..11] -> right, do not shift, [12..13] -> display on, cursor on
// [14..15] -> write char 'B'
unsigned int txData[] = {0x03, 0x03, 0x03, 0x02, 0x02, 0x00, 0x00, 0x08, 0x00, 0x01, 0x00, 0x06, 0x00, 0x0F, 0x24, 0x22};
void main() {
WDTCTL = WDTPW | WDTHOLD;
// for i2c pins
P1SEL = 0xC0;
P1SEL2 = 0xC0;
// i2c config
UCB0CTL1 |= UCSWRST;
UCB0CTL0 = UCMST | UCMODE_3 | UCSYNC;
UCB0CTL1 = UCSSEL_3;
UCB0BR0 = 12;
UCB0BR1 = 0;
UCB0I2CSA = 0x27; // slave address
UCB0CTL1 &= ~UCSWRST;
// enable tx interrupt
IE2 |= UCB0TXIE;
_enable_interrupts();
// start to transmit data
ptxData = txData;
UCB0CTL1 |= UCTR + UCTXSTT;
while (1);
}
#pragma vector = USCIAB0TX_VECTOR
__interrupt void USCIAB0TX_ISR(void){
// send txData elements one by one
UCB0TXBUF = *ptxData;
count++;
*ptxData++;
// if txData ends, start from beginning
if (count == 16) {
count = 0;
ptxData -= 16;
}
}
What am I missing, can you help me?