Part Number: MSP430FR2111
Hello, I have certain functionality that I need to achieve but want to choose the lowest power mode. I do not have any external crystals connected so I am limited to internal clock sources
Only using 2 peripherals (ADC and UART) and want to achieve lowest power possible by turning off peripherals when not in use and select appropriate clock sources.
a. Using the ADC at 3Hz, sampling 2 channels. What clock source should I use?
b. UART bus at 9600 baud. 32 bits of data is requested at 2Hz from the MSP430 over this bus
Thanks,
E