This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432E401Y: EEPROM address range and programming/erasing

Part Number: MSP432E401Y

Hi,

I am working with the MSP432E401Y device and I have a question about EEPROM usage(in meaning of programming/erasing). In the datasheet, I can see, that MSP432E401Y has the 1024kB of flash memory(memory range 0x0 - 0xF_FFFF) and the 6kB of EEPROM memory. 

1. What is the address range for EEPROM memory? I can;t see the details in reference manual/datasheet.

2. Can be the EEPROM programmable as the main flash(i.e. 32-word flash memory write buffer) directly via SWD interface?

Best regards,

Tomas

**Attention** This is a public forum