This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR5962: Time measurement during the low power mode

Part Number: MSP430FR5962


Hello, I am currently using a Msp430FR5962 controller. I put this in LPM3 mode (see code):

    // Clock System Setup
     CSCTL0_H = CSKEY_H; // Unlock CS registers
     CSCTL1 = DCOFSEL_0; // Set DCO to 1 MHz
     CSCTL2 = SELM__DCOCLK | SELS__DCOCLK | SELA__VLOCLK;
     CSCTL3 = DIVA__1 | DIVS__1 | DIVM__1; // Set all dividers to 1
     CSCTL4 = LFXTOFF | HFXTOFF;
     CSCTL0_H = 0; // Lock CS registers

     __bis_SR_register (LPM3_bits | GIE);

I would like to switch the MSP to low power mode and count (measure) the time until the MSP leaves the low power mode. The VLOCLK runs with the above code, but it is very imprecise and not temperature-stable.
What options do I have to put the MSP into a very low power mode and still measure a time with an approximate accuracy of + -1ms. Also over the temperature range from -40 ... + 85 ° C.

Furthermore, this clock generator must also start to oscillate relatively quickly, in a maximum of 5 to 10 ms.

What are my options?

**Attention** This is a public forum