This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430F5528: DriverLIB/MSPWARE help

Part Number: MSP430F5528


Tool/software: Code Composer Studio

Hi, 

I'm using the GPIO API included with driver Lib to turn ports 5.2/5.3/j.0/j.1 on, and I can't get them to turn on. I've connected LED's to them to ensure if they're turning on or not and can see that they're not. Here's the code: 

#include "driverlib.h"

#include <msp430.h>

void main (void)

{

    //Stop WDT

    WDT_A_hold(WDT_A_BASE);

    //PA.x output

    GPIO_setAsOutputPin(GPIO_PORT_P5, GPIO_PIN2+GPIO_PIN3);

    GPIO_setAsOutputPin(GPIO_PORT_PJ, GPIO_PIN0+GPIO_PIN1);

    //Set all PA pins HI

    GPIO_setOutputHighOnPin(GPIO_PORT_P5, GPIO_PIN2+GPIO_PIN3);

    GPIO_setOutputHighOnPin(GPIO_PORT_PJ, GPIO_PIN0+GPIO_PIN1);

    P1DIR |= 0x01;                  // configure P1.0 as output

    volatile unsigned int i;        // volatile to prevent optimization

    while(1)

        {

            P1OUT ^= 0x01;              // toggle P1.0

            for(i=10000; i>0; i--);     // delay

        }

    //Enter LPM4 w/interrupts enabled

    __bis_SR_register(LPM4_bits + GIE);

    //For debugger

    __no_operation();

}

**Attention** This is a public forum