Other Parts Discussed in Thread: UNIFLASH
Hi,
This is my first time using this development board (EVM430-FR6047). And I've followed the tutorial like this document :
https://www.ti.com/lit/slau810
I tried flashing the image in 2 ways.
Command : >> MSP430Flasher.exe -w C:\ti\msp\UltrasonicWaterFR604x_02_40_00_00\image\MSP430FR6047EVM_USS_Water_Demo_LPM_02_40_00_00.txt
NB : the image file I'm using is the example file from here :
Both methods are successful in flashing the firmware, but a few moments later the error indicator on the board (LED03) lights up red. And when I checked using USSDesignCenter, there was an error description like this.
What is the cause of this error ?, and how to fix it ?.
Thank you very much