Other Parts Discussed in Thread: MSP430F2274
Hello,
I have an MSP430F2274 I am putting in LPM4. When I initially did this, I measured the current draw in LPM4 to be <0.7uA. Next, I wanted to use P2.6 as a general purpose input and wake up on a signal transition interrupt. So, I set P2SEL to 0x80 and enabled the interrupt, and now when I am in LPM4, the current draw is more than 7uA! The only difference between these two measurements is the clearing BIT6 of P2SEL to use it as an input. The electrical connection to pin P2.6 remain the same. I have pin P2.6 externally pulled up to VCC with a 100k resistor, and another device's open-drain output connecting to the circuit.
Does anyone know why changing P2.6 from XIN to a general purpose input would cause such a large change in current? This isn't the case for other GPIO pins I'm using as inputs...
Thanks