Other Parts Discussed in Thread: LP3961
I'm writing my master thesis in the field of electrical engineering and I've come across a small problem which is simply unclear to me.
I use a battery to power my microcontroller and I used a MCP1700 LDO to get a constant 3,3V supply ( data sheet pdf1.alldatasheet.com/.../MCP1700.html )
Because the current range didn't quite fit I have now switched to the LP3961 in the 3.3V version. Input and output are each connected with a 100uF capacitor as requested in the data sheet. ( Datenblatt www.ti.com/.../snvs056j.pdf
The problem:
the MCP makes clean 3.29V at the output everything as it should be...
The LP, however, gives me 3.59V and this not really clean, the LEDs on my microcontroller flicker and sometimes the whole thing hangs up.
What can be the solution here ? is the LP just broken ? I am really at the end of my knowledge, unfortunately I only have the one.
Hope someone has a tip
Translated with www.DeepL.com/Translator (free version)