Part Number: MSP430F169
Tool/software: TI C/C++ Compiler
Hello everyone, I am programming the MSP430F169, for industrial applications such as measurement of variables via ADC.
My drawback is the following when I am at room temperature all the measurements are correct, but when there is a high or low temperature change. Measurements seem to deviate a bit from the real thing.
I would like to know if there is any hardware or software way that allows me to calibrate the ADC module based on temperature. I can measure the internal temperature of the microcontroller and from there I would do a recalibration of the module.
If you have information about this, it would be of great help.
Thank you.
Regards,