Part Number: MSP430-GCC-OPENSOURCE
Tool/software: TI C/C++ Compiler
Compiled with MSP430-GCC 9.2.0.0
flags:
CFLAGS = -mmcu=$(MCU) -std=gnu11 -g -Os -fno-ipa-icf-functions \
-Wall -Wunused -ffunction-sections -fdata-sections -fomit-frame-pointer -fwrapv -MMD
The source code just determines whether to transmit another packet or stop.
__attribute((interrupt))
void xmit_char_3(void)
{
UCA0TXBUF_L = uart_txbuf.buff[3];
if(uart_tx_msg_sent != uart_tx_msg_pending)
IRQ_UART_TX = uart_tx_next;
else
IRQ_UART_TX = RETI;
}
The resulting assembler. Notice that the target of the bolded jump is just RETI.
In this case, the compiler should have simply emitted RETI, saving this handler 2 clock cycles.
0xe7fe: 0x42d2 mov.b &0x2569, &0x050e 6
0xe800: 0x2569
0xe802: 0x050e
0xe804: 0x9292 cmp.w &0x2564, &0x2562 6
0xe806: 0x2564
0xe808: 0x2562
0xe80a: 0x2404 jeq 0xe814 (offset: 8) 2
0xe80c: 0x4292 mov.w &0x2002, &0x27d6 6
0xe80e: 0x2002
0xe810: 0x27d6
0xe812: 0x1300 reti 5
0xe814: 0x40b2 mov.w #0xff88, &0x27d6 5
0xe816: 0xff88
0xe818: 0x27d6
0xe81a: 0x3ffb jmp 0xe812 (offset: -10) 2