This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR5969-SP: ADC input limit & EOS damage

Part Number: MSP430FR5969-SP

Hello team,

My customer is using MSP430FR5969-SP in their design.  They have concerns of the if they are using the 2.5 V reference built into the MSP430 (as the analog reference) and the analog signal goes above that (but still below the MSP430 operating voltage (3.3 V), will damage result to the device? 

An example of ADC input amplitude rising to 3.05 V.

Thank you in advance for your support!

Errol

**Attention** This is a public forum