Part Number: MSP-GANG
Hi,
After opening the software and connecting the MSP-GANG for the first time, I was prompted to update the firmware of the programmer, which I accepted. There was no visual feedback, so I waited a while and unplugged/replugged the programmer, which must have interrupted the firmware update process. Now the LCD is blank and the MSP-Gang software can't connect to it. I only get these error messages:
ERROR 3: API Firmware CRC error! The API Firmware should be reloaded.
ERROR 322: Command failed or not defined or Target not accessible !
How can I push the correct firmware in the GANG-Programmer?