Part Number: MSP430G2553
Other Parts Discussed in Thread: MSP430G2533
Hi,
I have obtained the above screen shot from MSP4302553 DataSheet. I am trying to monitor the discharge time of a capacitor by using an interrupt on a GPIO . I have configured the IES to be High-Low interrupt.
I have the signals being monitored on a PICOSCOPE and I realize that the interrupt on the gpio is being triggered at appx. 1.32V .
Please explain what the 'MIN' and "MAX" Exactly mean in the above highlighted numbers. Does it mean there can be two trigger points ?
I want to set the interrupt to be triggered at 0.75V .
Thank you,