This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430F5638: How to speed up the refresh speed of LCD?

Part Number: MSP430F5638


Tool/software: Code Composer Studio

Dear team,

1 The customer uses a 1.54-inch color screen, a resolution of 240×240 and an 8-bit parallel port. He found that the refresh rate is very slow.

   What solutions are there?

2 The customer also wants to use LCD which screen is 4.0 inches and the resolution is 480×800. Is it possible?

BR,

Susan

**Attention** This is a public forum