This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR2355: Reporting typo in manual

Part Number: MSP430FR2355

Where can I report a minor typo in the user manual for a TI part?

============================================================

"Literature Number: SLAU445I
October 2014–Revised March 2019", the MSP430FR2xxx manual as follows:

Where it reads UMODEx, it should read UCMODEx:

22.3.4.1 Transmitting a Break/Synch Field
The following procedure transmits a break/synch field:
1. Set UCTXBRK with UMODEx = 11.
2. Write 055h to UCAxTXBUF. UCAxTXBUF must be ready for new data (UCTXIFG = 1).

**Attention** This is a public forum