Part Number: MSP430FR6877
I am using an interrupt on a pin in port 4 and TA0 timer interrupt. I want the timer interrupt when it comes to interrupt the port interrupt. Is there a way to setup the interrupts priority so that the timer is higher priority than the port? Is even the interrupts nesting supported?