Part Number: MSP-EXP432E401Y
PAGE 12 and 13
J6, going down, starts at Pin 20 on the board. It is a GND, on the circuit board.
J6, going down, starts at Pin 11 in the tech data. It is listed as a GND, but it is not.
If you look at the tech data to hook up your own electronics, you'll attach GND toJ6 pin 11, which is NOT a GND on the board. Pin11 of J6 on the devkit is PM6 and is on the bottom of the connector, not the top. The numbers of the pins listed on the table 3 for J6 are not correct. in the pdf file, 11 is swapped with 20, 12 with 19, and so on.