Hi experts,
My customers is evaluating the SD24 and the conversion result is different for one channel (CH4) than the other channels.
I would appreciate any information you can provide.
Q: When I perform A/D conversion with CH4 and other channels at the same time, the result is about 0.3% larger than the result when I performed A/D conversion with CH4 alone.
Is the above behavior expected?
We are comparing a pattern in which CH4 is operated simultaneously with other channels (CH1, CH2, CH3 and CH6 grouped together and operated by continuous conversion) and a pattern in which CH4 is operated independently by continuous conversion.
If the above information is not enough, could you please tell us what information we should check?
(Register settings are being checked.)
Best regards,
O.H