Part Number: MSP430FR6047
Other Parts Discussed in Thread: EVM430-FR6047
Tool/software: Code Composer Studio
I want to calibrate the ultrasonic flow sensor with the GUI for water flow measurement (ultrasonic sensing design center) but the general calibration does not return a new meter constant. Neather it gives an other Mean VFR value than 0. I added corresponding screenshots. Maybe the data transport between my chip and the computer does not work correctly. Or it does not calculate anything at all. However, the program does not generate an error.
In addition to that all return values of a VFR Flow+Temperature measurement are zero.
I was able to configure the EVM430-FR6047 board and got waveform, capture and frequency sweep graphs that were reacting to changes of my configuration. So there is some connection between the GUI and my board.
I added additional information about my compter.
Please give me advice to solve this problem.
I also have some questions about the Ultrasonic Sensing Design Center itself. For the general calibration the program asks for the expected volume flow rate and after measuring for the average flow rate of my reference flowmeter. What is the difference between these two values? After all I am not changing the flow during the calibration.
The meaning of the meter calibration parameters are explained in the description of the Design Center. For Slope and Offset there is exactly the same explenation in the Design Center. So what is the difference between them both?
Please explain this to me. If there is a file that specially treates the calibration of the ultrasonic flow sensor, please send me the corresponding link.
Now, there is an other problem. I started with the Code Composer Studio and tried a self-written "hello world" program. Unfortunately I have not found an example project for this.
The problem is, that I have not found the original firmaware (default or demo firmware) to reset the board and continue the measurement. Where do I find it? I would also need the project archive to learn from the original code.
I would be glad for answers for any of my problems.
Best regards,
Kathrin