Part Number: MSP430FR2422
Tool/software: Code Composer Studio
Dear Sir,
I have configured for PWM generation. But signal is not available at P2.3 port pin.
please find below code.
int main(void)
{
WDTCTL = WDTPW | WDTHOLD;
PM5CTL0 &= ~LOCKLPM5;
OutPutPortConfiguration();
TimerB0_Configuration();
PWMGeneration();
while(1)
{
__bis_SR_register(LPM0_bits | GIE);
__no_operation();
__delay_cycles(500);
}
}
void OutPutPortConfiguration(void)
{
P2DIR |= BIT3; //P2.2 and P2.3
P2OUT &=~BIT3;
P2SEL0 |= BIT3;
P2OUT |= BIT3;
}
void TimerB0_Configuration(void)
{
TA0CTL |= TACLR; //before start clear the TimerA
TA0CTL |= MC__UP; //UP Counter
TA0CTL |= TASSEL__ACLK; //32768HZ
}
void PWMGeneration(void)
{
TA0CCR0 = 32768; //PERIOD is 1 Seconds
TA0CCR1 = 16384; //DUTYCYCLE is 500 MS
TA0CCTL0 |=CCIE;
TA0CCTL0 &=~CCIFG;
TA0CCTL1 |=CCIE;
TA0CCTL1 &=~CCIFG;
TA0CCTL0 |= OUTMOD_7;
TA0CCTL1 |= OUTMOD_7;
}
#if 1
#pragma vector = TIMER0_A0_VECTOR
__interrupt void ISR_TA0_CCR0(void)
{
//P2OUT |= BIT3;
TA0CCTL0 &=~CCIFG;
__bic_SR_register_on_exit(LPM0_bits);
}
#pragma vector = TIMER0_A1_VECTOR
__interrupt void ISR_TA0_CCR1(void)
{
//P2OUT &= ~BIT3;
TA0CCTL1 &=~CCIFG;
__bic_SR_register_on_exit(LPM0_bits);
}
#endif