I am trying to use the Fet-Pro430 lite to load the .out file that I have created in CC4. I can use the CC4 debugger and load the code just fine and debug it. I'm trying to use the
FET-Pro430 lite so that I don't have to use the debugger to load. I can get into the FET-Pro430 lite and do a Verify. This works and verifies okay. It shows me that my target
is MSP4302274. So I go to group and I set it to MSP4302xx and below that set it to MSP4302274. When I try to program or verify, I get the following error:
The FET-Pro430 free version works only with Texas Instruments' FET adapters. If the 3-th party adapter is used, then the Fet-Pro430 should be used.
Is there no way to do what I am trying to do with the lite version? Or I is there something else I am doing wrong?
Any help would be greatly appreciated.
Thanks,
Gary Lanehart