Tool/software: Code Composer Studio
I'm use MSP430FR2433 to make sure other devices are working properly.
The device operates at 400Hz.
So I should be able to measure 0.0025 seconds to find the error.
I tried using ACLK, but it wasn't accurate enough. result was varying for each MSP chip.
DCO, MCLK is 16MHz.
How can I time accurately and precisely?
Thank in advance.