Part Number: MSP430F6779A
So, I have been trying to receive some digital inpits bits connected to the I/O expander using I2C. The code worked once few months ago, but now when I am trying again it isn't working. When I added a breakpoint in my interrupt vector table for NACK interrupt flag, I found the microcntroller is getting a NACK flag. I am 100% sure that the slave address is correct (0x19). I have enabled all the interrupts, but the code get stuck in a while loop when I try to recieve byte information. This shows that the connection between the master and slave is not established and it is causing the problem. I have tried everything to make it work, but it isn't working. Please help me out here.
The part where I am getting stuck is below. When I try to recieve the byte in the mains while loop, the code get stuck in the EUSCI_B_I2C_masterReceiveSingle while loop. When I try to call the same function in the interrupt as shown in the code below, the controller doesn't reach that statement because RXIFG bit is not set.
uint8_t EUSCI_B_I2C_masterReceiveSingle(uint16_t baseAddress)
{
//Polling RXIFG0 if RXIE is not enabled
if(!(HWREG16(baseAddress + OFS_UCBxIE) & UCRXIE0))
{
while(!(HWREG16(baseAddress + OFS_UCBxIFG) & UCRXIFG0)) // the code get stuck here
{
;
}
}
//Read a byte.
return (HWREG16(baseAddress + OFS_UCBxRXBUF));
}
This is my whole code for receiving data through I2C
#define SLAVE_ADDRESS 0x19
#include "driverlib.h"
uint8_t RXData;
void main(void)
{
//Stop WDT
WDT_A_hold(WDT_A_BASE);
GPIO_setAsPeripheralModuleFunctionInputPin(
GPIO_PORT_P4,
GPIO_PIN4 + GPIO_PIN5
);
EUSCI_B_I2C_initMasterParam param = {0};
param.selectClockSource = EUSCI_B_I2C_CLOCKSOURCE_SMCLK; //Setting clock source to SMCLK
param.i2cClk = UCS_getSMCLK();
param.dataRate = EUSCI_B_I2C_SET_DATA_RATE_100KBPS;
param.byteCounterThreshold = 1; //Number of bytes to receive
param.autoSTOPGeneration =
EUSCI_B_I2C_NO_AUTO_STOP; //No auto stop. I can set it to stop if the desired bytes ( in this case - 1) is received.
EUSCI_B_I2C_initMaster(EUSCI_B1_BASE, ¶m);
EUSCI_B_I2C_setSlaveAddress(EUSCI_B1_BASE,
SLAVE_ADDRESS
);
//Set Master in receive mode
EUSCI_B_I2C_setMode(EUSCI_B1_BASE,
EUSCI_B_I2C_RECEIVE_MODE
);
UCB1IE = 0;
//Enable I2C Module to start operations
EUSCI_B_I2C_enable(EUSCI_B1_BASE);
EUSCI_B_I2C_clearInterrupt(EUSCI_B1_BASE,
EUSCI_B_I2C_RECEIVE_INTERRUPT1 +
EUSCI_B_I2C_BYTE_COUNTER_INTERRUPT + EUSCI_B_I2C_NAK_INTERRUPT); //Clearing all required interrupts
EUSCI_B_I2C_enableInterrupt(EUSCI_B1_BASE,
EUSCI_B_I2C_RECEIVE_INTERRUPT1 +
EUSCI_B_I2C_BYTE_COUNTER_INTERRUPT + EUSCI_B_I2C_NAK_INTERRUPT
);
__enable_interrupt();
//__bis_SR_register(GIE);
while(1)
{
__delay_cycles(2000);
while(EUSCI_B_I2C_SENDING_STOP ==
EUSCI_B_I2C_masterIsStopSent(EUSCI_B1_BASE))
{
;
}
// I2C start condition
EUSCI_B_I2C_masterReceiveStart(EUSCI_B1_BASE);
}
}
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=USCI_B1_VECTOR
__interrupt
#elif defined(__GNUC__)
__attribute__((interrupt(USCI_B1_VECTOR)))
#endif
void USCIB1_ISR(void)
{
static uint8_t count = 0;
switch(__even_in_range(UCB1IV,0x1E))
{
case 0x00:
break; // Vector 0: No interrupts break;
case 0x02: break; // Vector 2: ALIFG break;
case 0x04:
EUSCI_B_I2C_masterReceiveStart(EUSCI_B1_BASE);
break; // Vector 4: NACKIFG break;
case 0x06: break; // Vector 6: STT IFG break;
case 0x08: break; // Vector 8: STPIFG break;
case 0x0a: break; // Vector 10: RXIFG3 break;
case 0x0c: break; // Vector 14: TXIFG3 break;
case 0x0e: break; // Vector 16: RXIFG2 break;
case 0x10: break; // Vector 18: TXIFG2 break;
case 0x12:
RXData = EUSCI_B_I2C_masterReceiveSingle(
EUSCI_B1_BASE
);
break; // Vector 20: RXIFG1 break;
case 0x14: break; // Vector 22: TXIFG1 break;
case 0x16:
RXData = EUSCI_B_I2C_masterReceiveSingle(
EUSCI_B1_BASE
); // Get RX data
break; // Vector 24: RXIFG0 break;
case 0x18: break; // Vector 26: TXIFG0 break;
case 0x1a:
break; // Vector 28: BCNTIFG break;
case 0x1c: break; // Vector 30: clock low timeout break;
case 0x1e: break; // Vector 32: 9th bit break;
default: break;
}
}
Please help me, I am ot sure what I am doing worng. I have spent weeks now trying to figure this out.Pls help. Thanks