This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR6043: problem with TOF time measurement

Part Number: MSP430FR6043


Hello. I use MSP430FR6043 evaluation board with MSW-A10400H07TR-W (400kHz) ultasonic sensors. I use Trans-Axial tube design. Settings you can see in the attachments file.


The problem is: when I start to measure flow with 5l/sec glow rate I receive the following (attachments file). The experiment: at first I measure flow in one direction and then the opposite direction.
Please, tell me why TOF time turnes to zero after 10microseconds of evaluation? Maybe I have some wrong settings?

**Attention** This is a public forum