Part Number: MSP430FR2355
Other Parts Discussed in Thread: MSP430G2553
Tool/software: Code Composer Studio
Hello, I'm implementing SPI communication using msp430fr2355, I need this in order to interface a CAN controller. I'm using examples from resource explorer for my SPI driver, and I'm using drivers
I've already implemented using msp430g2553 to program the controller and the CAN communication, so I just need to port my SPI driver for the new microcontroller (msp430fr2355)
This is my code for SPI driver:
unsigned char tx_a0_data;
unsigned char rx_a0_data;
void SPI_init()
{
P1SEL0 |= BIT5 | BIT6 | BIT7; // set 3-SPI pin as second function
UCA0CTLW0 |= UCSWRST; // **Put state machine in reset**
UCA0CTLW0 |= UCMST|UCSYNC|UCCKPL|UCMSB; // 3-pin, 8-bit SPI master
// Clock polarity high, MSB
UCA0CTLW0 &= ~UCSSEL_1;
UCA0CTLW0 |= UCSSEL__SMCLK; // Select SMCLk = 24Mhz
UCA0BR0 |= 24; //Transmission clock 1Mhz
UCA0BR1 = 0; // .-
UCA0MCTLW = 0; // No modulation
UCA0CTLW0 &= ~UCSWRST; // **Initialize USCI state machine**
UCA0IE |= UCRXIE;
}
unsigned char SPI_transmit(unsigned char data)
{
tx_a0_data = data;
UCA0IE |= UCTXIE; // Enable TX interrupt
return rx_a0_data;
}
#pragma vector=EUSCI_A0_VECTOR
__interrupt void USCI_A0_ISR (void)
//interrupt [UART0TX_VECTOR] void UART0_TX_ISR (void)
{ //ToDo: Generalize this interruptions
switch(__even_in_range(UCA0IV,USCI_SPI_UCTXIFG))
{
case USCI_NONE:
break; // Vector 0 - no interrupt
case USCI_SPI_UCRXIFG:
rx_a0_data = UCA0RXBUF;
UCA0IFG&=~UCRXIFG;
break;
case USCI_SPI_UCTXIFG:
UCA0TXBUF = tx_a0_data;
UCA0IE &= ~UCTXIE;
break;
default: break;
}
}
I have a question in this code, specifically about the spi clock configuration, I have the microcontroller's clock configured like this:
void init_clock(void)
{
/// Configure two FRAM waitstate as required by the device datasheet for MCLK
// operation at 24MHz(beyond 8MHz) _before_ configuring the clock system.
FRCTL0 = FRCTLPW | NWAITS_2 ;
P2SEL1 |= BIT6 | BIT7; // P2.6~P2.7: crystal pins
do
{
CSCTL7 &= ~(XT1OFFG | DCOFFG); // Clear XT1 and DCO fault flag
SFRIFG1 &= ~OFIFG;
} while (SFRIFG1 & OFIFG); // Test oscillator fault flag
__bis_SR_register(SCG0); // disable FLL
CSCTL3 |= SELREF__XT1CLK; // Set XT1 as FLL reference source
CSCTL0 = 0; // clear DCO and MOD registers
CSCTL1 |= DCORSEL_7; // Set DCO = 24MHz
CSCTL2 = FLLD_0 + 731; // DCOCLKDIV = 24MHz
__delay_cycles(3);
__bic_SR_register(SCG0); // enable FLL
while(CSCTL7 & (FLLUNLOCK0 | FLLUNLOCK1)); // FLL locked
CSCTL4 = SELMS__DCOCLKDIV | SELA__XT1CLK; // set XT1 (~32768Hz) as ACLK source, ACLK = 32768Hz
// default DCOCLKDIV as MCLK and SMCLK source
// P1DIR |= BIT0 | BIT1 ; // set ACLK SMCLK and LED pin as output
// P1SEL1 |= BIT0 | BIT1; // set ACLK and SMCLK pin as second function
}
I understand my SMCLK is 24Mhz, so in the code above, my spi clock is configured for 1Mhz. Is it correct?
I'm trying to do the same configuration I had with the msp430g2553, this was the code in that case:
void init_CLK(){
BCSCTL1 = CALBC1_8MHZ; //BCSCTL1 Calibration Data for 1MHz
DCOCTL = CALDCO_8MHZ; //DCOCTL Calibration Data for 1MHz
BCSCTL2|=SELM0+DIVM_0; //MCLK sourced from DCO DIV/1
BCSCTL2&=~SELS; //SMCLK sourced from DCO
BCSCTL2=DIVS_2; //SMCLK DIV/4
}
void msp430_SPI_init(uint8_t USCIX)
{
UCA0CTL0=0x00; // Clear the contents of the register
//using USCI A0 (Universal Serial Communication Interface)
UCA0CTL1 |= UCSWRST; // Reset
UCA0CTL0 |= UCCKPH + UCMST + UCMODE_0 + UCSYNC; // 3-pin, 8-bit SPI master
UCA0CTL0|=UCMSB; //MSB FIRST
UCA0CTL0&=~UC7BIT; // Data for 8 Bit
UCA0CTL1 = 0x00; // Clear content of register
UCA0CTL1 |= UCSSEL_2; // SMCLK
UCA0CTL1 &= ~UCSWRST; // Initialize USCI state machine
UCA0BR0 |= 0x02; //Transmission clock SMCLK / 2
UCA0BR1 = 0; // .-
// No modulation
IE2|= UCA0RXIE + UCA0TXIE; //USCI_A0 receive/transmit interrupt enable
IFG2 &=~UCA0TXIFG; //clear flag, no Interrupt pending
P1SEL = BIT1 | BIT2 | BIT4; // P1.1 SOMI - P1.2 SIMO - P1.4 SCK
P1SEL2 = BIT1 | BIT2 | BIT4;
}
I understand in that case, the SMCLK was configured to work at 8Mhz/4 and finally spi clock in 1Mhz. Then the configurations of spi clock for both microcontrollers
would be the same. Is this right or am I doing or understanding something wrong in the configurations?
The CAN controller is programmed via SPI. Right now, my CAN communication is not working with the msp430fr2355 then I suppose my SPI driver is not working and I'm not able to program the controller correctly.
I hope you can help me, thanks in advance.
Regards,
Diana