Given that you have to enable interrupts what is the value of the break statement in the UCRXIFG and UCTXIFG below? Doesn't it stand to reason that if I did NOT have the break in the UCRXIFG and did NOT have the UCTXIE enabled that I would still return at the end of the case of UCRXIFG? I understand that in a normal case statement that you would go through all the cases if you didn't use a break statement but given that enables are used here it seems that breaks are unnecessary??
#pragma vector=USCI_A1_VECTOR //radio communication
__interrupt void RF_ISR_USCIA1(void)
{
switch(__even_in_range(UCA1IV, USCI_UART_UCTXIFG))
{
case USCI_NONE: break;
case USCI_UART_UCRXIFG:
*rxMssg = UCA1RXBUF;
rxMssg++;
rxCount++;
LPM3_EXIT;
break;
case USCI_UART_UCTXIFG:
LPM3_EXIT;
break;
default: break;
}
}