I have an application that I want to boot into LPM3 with P1.1 enabled as a switch....Upon pushing this switch I want a PWM to operate AND I enable the RTC at once per second. I exit P1 interrupt still sleeping. The hope is that after 100 seconds a counter in the RTC recognizes this and puts the device into LPM3.5. Upon coming out of 3.5 I attempt to clear PMMREGOFF and force a brownout which puts me back at 'normal' mode. None of this seems to be happening correctly....The code below after pushing the button starts the PWM then after about 2 seconds of flashing the LED just stays on. I am finding it EXTREMELY difficult to work with this LPM3.5/RTC. I constantly am trying to pause the debugger to reboot but CCS will have non of it and tends to lock up. Can someone give me suggestions on both what I am doing wrong in the code as well as why CCS keeps wanting to lock up? BTW. The RTC #2 program under this part and resource explorer does similar. I've cut and pasted it just changing the IO to my IO and CCS still wanders off. I have loaded the RTC #1 program onto the board and it works fine (every second it just toggles the IO in the RTC).
I would ultimately like to go into LPM3 after the PWM is over (my understanding is PWM won't work below LPM3) and reboot to a state of just very low power ie 3.5 until someone pushes the button again.
Thanks
CCS when pause is pushed responds with:
MSP430: Trouble Halting Target CPU: Internal error
#include <msp430.h>
#include "funct.h"
volatile unsigned int count;
volatile unsigned int flag = 0;
int main(void)
{
WDTCTL = WDTPW | WDTHOLD; // stop watchdog timer
//small macro to flash LED to show a reset has occured.
configGPIO();
PM5CTL0 &= ~LOCKLPM5;
__delay_cycles(80000);
P1OUT &= ~BIT4;
configACLK();
if (SYSRSTIV == SYSRSTIV_LPM5WU) { //wake up from LPM3.5?
flag = 0;
configGPIO();
PMMCTL0 = PMMPW;
PMMCTL0 &= ~PMMREGOFF; //clear LPM3.5 bit
PMMCTL0 |= PMMSWBOR; // force reboot to normal
}
else { //no?
__bis_SR_register(LPM3_bits + GIE); //LPM3.5 entry point
}
return 0;
}
#pragma vector = RTC_VECTOR
__interrupt void thirtyMinuteCounter(void)
{
switch(__even_in_range(RTCIV, RTCIV_RTCIF))
{
case RTCIV_NONE : break; // No interrupt pending
case RTCIV_RTCIF: // RTC Overflow
count++;
if (count >= 100)
{
count = 0;
PMMCTL0 = PMMPW; // Open PMM Registers for write
PMMCTL0_L |= PMMREGOFF; //sets LPM3.5
}
break;
default:
break;
}
}
#pragma vector = PORT1_VECTOR
__interrupt void ifNonLPM3_5(void)
{
switch (__even_in_range(P1IV, 4))
{
case 4: //P1.1
configTA0_PWM(16384, 4); //3276
configRTC(33); //1800
break;
default:
break;
}
}