This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR2422: Configuring UART in Port 2

Part Number: MSP430FR2422


Hi Team,

Posting on behalf of our customer. They are currently having issues in configuring port 2 of MSP430FR2422 as UART. Here is a full transcript of their query:

I set P2SEL0 ( bis.b ##BIT0+BIT1, &P2SEL0), to any happens, clr P2SEL1 - no any signal on pin P2.0. If I set bis.b #BIT4+BIT5,&P1SEL0 - I see the signal with the oscilloscope on pin P1.4, that I send to UART. When I configure the P2 to out (and clr P2SEL1 and P2SEL0) and send digital signal - I see this signal with the oscilloscope. Thus P2 work and UART work separately, but they don't work together. How can we make this work?

Thanks in advance!


Kind Regads,

Jejomar

**Attention** This is a public forum