Can someone tell me what I am doing wrong in this small block:
mssg = Send;
strcpy(Send, "HelloWorld");
m = strlen(mssg);
CRC_Result = CRC(mssg, m);
CRC_char[0] = (CRC_Result >> 8) & 0xFF;
CRC_char[1] = (CRC_Result & 0xFF);
mssg = (strcat(mssg, (const char*)CRC_char));
char *mssg, junk, CRC_char[2];
uint CRC_Result, m;
char Send[BUFFER_SIZE] = {[0 ... BUFFER_SIZE-1] = 0xFF};
BUFFER_SIZE = 30.
The CRC_Result has been verified and is good. It is an unsigned int. However when I do the concatentation I get the CRC added to the message AND then after that I get the byte swapped CRC added to the message. I have tried all kinds of variants and can't seem to find what I am doing wrong? If I concat a string constant like "Today" to my mssg it works fine. CRC_char looks as expected after CRC_Result.
Thanks