Other Parts Discussed in Thread: EVM430-CAPMINI, MSP430FR2512
Hi,
I am evaluating the MSP430FR2522 for use with an application that has two 3-element capacitive touch sliders. Due to space restrictions the sliders are very small, an overall area of around 8.5mm x 21mm for the 3 elements. The effective area of each element is around 38mm2. For testing a 3mm thickness acrylic sheet is used to be representative of the overlay in the eventual product design. I believe we have about 9 to 11pF parasitic capacitance and 0.2pF touch capacitance change with our touch slider PCB.
The application was previously using the Cypress CY8CM-BR3106S but for various reasons we want to migrate to the MSP430FR2522. The Cypress part was giving a sensible touch sensitivity with gain in hand but the MSP430FR2522 seems to be struggling to achieve enough sensivity, even with what I believe to be the parameters set for maximum sensitivity using the CapTIvate Design Centre. We are actually using an EVM430-CAPMINI eval board with the eval board button tracks cut and our slider PCB neatly wired to it instead. The MSP430GR2512 has been refitted with an MSP430FR2522 and re-programmed accordingly.
The Conversion Gain is set to 100 but the Conversion Count can't be set to more than 1800 otherwise the CapTIvate Design Centre reports an error that the Proximity or Touch threshold is too low. Does anyone know how the sensitivity can be increased without running into this problem?
Has anyone any experience of achieving adequate performance with the MSP430FR2512 or 2522 with the above mention touch/parasitic capacitance, or experience of comparing the Cypress solution with the MSP430?
Best regards,
Gerry