#!/usr/bin/python
""" Parses USS Template project UART data (src.csv) and store result in out.csv"""
import re
import struct
import sys
def decode_file(file_in_name, file_out_name):
""" Decodes input file using delim_dict and stores decoded output"""
delim_dict = {"$": "AbsTof-UPS", "#": "AbsTof-DNS", "%": "DToF", "!": "VFR"}
# Open File Input and Output Files
input_file = open(file_in_name, "r")
target_file = open(file_out_name, "w")
# Iterate through the data
for line in input_file:
# Remove New Line
line = line.rstrip("/n")
# Remove Spaces in front
line = line.lstrip(" ")
# Remove White space and tabs
pattern = re.compile(r"\s+")
clean_line = re.sub(pattern, " ", line)
# Split the line by spaces
line_list = clean_line.split(",")
# Check if the first Value is supported by dictionary
if line_list[0] in delim_dict.keys():
target_file.write(delim_dict[line_list[0]])
else:
target_file.write("Undefined " + line_list[0])
target_file.write(",")
result = struct.unpack("f", struct.pack("I", int(line_list[1], 16)))[0]
# Format the output in exponent notation
target_file.write("{0:e}".format(result) + "\n")
# Close Files
input_file.close()
target_file.close()
print("Successfully Generated: \n", file_out_name)
return
if __name__ == "__main__":
if len(sys.argv) != 3:
print "Invalid input. Usage uart_parser.py <input_csv> <output_csv>"
else:
# Parse the USS Template project src input file and store result in
# output csv
decode_file(sys.argv[1], sys.argv[2])
/