Part Number: MSP430FG4617
Hi there!
I'm designing the PCB layout for MSP430FG4617 microcontroller and I have a silly question (or maybe not).
I'm connecting DVCC pins (pin 1 and pin 60) separately from my source but I wonder if they also should be connected together. For example, with a new trace below de uC that connects pin 1 and pin 60.
Is this necessary?
Also, I'm using 8mil trace by default. It's recommended to use wider traces for DVCC since supply it's only 3.6V?
Thank you for your time.
Regards,
Pedro.