This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVM430-FR6047: TIDA-01486 standard USS software

Part Number: EVM430-FR6047
Other Parts Discussed in Thread: TIDA-01486

Hello,

I would like to use the TIDA-01486 as Booster to develop a flow meter for steel pipes with larger diameter. 
I found in other threads to replace 4 files to be able to use the standard USS software to run the EVM with the TIDA-01486 BoosterPack. 

Regarding this i have 2 questions:

1) Is the replacement of these files necessary in the newest software release (USS_02_40_00_00)? I wonder because the Param10 which was mentioned here:  is already included.

2) If is use the original reference design for the TIDA-01486 which adjustments at the EVM is needed and what is necessary to connect both?

**Attention** This is a public forum