Part Number: MSP430FR5962
Hi,
I would like to have the clock output from the IO port of MSP430FR5962.
Q1:Can the IO port of MSP430FR5962 output a 4MHz clock?
Datasheet specifies the minimum value of the clock output as 16MHz, but could it be a mistake for the maximum value?
Q2:Can this clock output be used as a reference clock for external devices?
(Can you provide accuracy information such as jitter?)
Best Regards,
UNA