This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F6638: Does the ZCA package have TA0?

Part Number: MSP430F6638

Hello.

When I look in section 9.12.11 of the datasheet there is a table that shows Timer TA0 has a PIN NUMBER for just the ZQW package, but the next section 9.12.12 for TA1 shows the pinouts for both ZCA and ZQW packages. Is this an error in the datasheet? My understanding is that the two packages are pinned out identically.

Also, when I look at Section 7.2 Signal Description, it seems no difference between ZCA package and ZQW package in pin definition. So my question is if Timer TA0 is an active function in MSP430F6638IZCA?

Thanks!

John

 

**Attention** This is a public forum