Other Parts Discussed in Thread: MSP-EXP430F5529LP, MSP-ISO
Tool/software: Code Composer Studio
Dear Sir,
Part umber : MSP430F67791A
Code : EMDC Generated code
Baud rate : 250Kbps
I want to read all parameters data from EMDC through uart communication. I sent to EMDC on following commands are 0x55,0xAA,0X06,0X04,0X01,0X01,0X01,0X07,0X00 and EMDC reply the lot of data's.
Example: Received Phase A data is 0x55,0xAA,0X0A,0X04,0X80,0X01,0X01,0X60,0X3C,0X00,0X00,0X22,0X01 = 230V (how to calculate)
Now I connect Phase A only for input voltage 230V and output 542mV AC apply the SD0P0, SD0N0 pin in MSP430F67791A Mcu.