Part Number: MSP430FR6877
Hello,
I couldn't understand about condition 2-(3) in PMM32 errata.
>Neither MODCLK nor SMCLK are running (e.g. requested by a peripheral)
Which Is it means in below?
1.All the time while throughout both of MODCLK and SMCLK are not running
2.When there is a request from either CLK when both MODCLK and SMCLK are not running
If your answer is 2 described above, is my understanding correct that SMCLK mentioned in condition 2-(3) in PMM32 errata is only triggered by ADC, eUSCI, ESI according to PMM31 errata?
If we don't use these module(ADC, eUSCI, ESI), Doesn't PMM32 issue occur?
Regards,
U-SK