Part Number: MSP-FET
Other Parts Discussed in Thread: RF430FRL152HEVM, , UNIFLASH, RF430FRL152H
Tool/software: Code Composer Studio
I am encountering the "Unknown device" error trying to flash/debug an RF430FRL152HEVM board using an MSP-FET when running CCS on Linux, but the exact same hardware setup works on Windows.
My Linux machine is running Ubuntu 20.10, CCS v10.1.1. I have also tried using MSPFlasher (result below) and UniFlash with no success.
jason@galvani:~/ti/MSPFlasher_1.3.19$ MSP430Flasher -s /home/jason/Work/s3-firmware/Debug/s3-firmware.txt -v -g * -----/|-------------------------------------------------------------------- * * / |__ * * /_ / MSP Flasher v1.3.19 * * | / * * -----|/-------------------------------------------------------------------- * * * Evaluating triggers...done * Checking for available FET debuggers: * Found USB FET @ ttyACM0 <- Selected * Initializing interface @ ttyACM0...done * Checking firmware compatibility: * FET firmware is up to date. * Reading FW version...done * Setting VCC to 3000 mV...done * Accessing device... # Exit: 16 # ERROR: Unknown device
I have checked that the `70-mm-no-ti-emulators.rules` file appears in `/etc/udev/rules.d` after running the post-installation script, and have tried reboots & not using a USB hub.
My Windows machine is running Win10 and CCS 9.3.0.