Hi,
When the internal reference power supply is selected and the gain is set to PGA = 1,
Is the full scale level at the time of differential input correct with the understanding of 1.84Vp-p?
In other words, is the + side converted to +920 mV and the minus side converted to -920 mV without being clipped?
Best Regards,