Looking to use the SEEED connector on the EVM. It is connected to A1 and A4.
First question....Does this particular MSP offer the ability to do repeated conversions on multiple channels that are not ordered? for instance A1, A4, A2? I know some of the MSP offer the ability to stack A/Ds in an order that is different than A1, A2, A3, A4, etc..... It appears not
Question two.....If I cannot just sample A1 and A4 WITHOUT A2 and A3....how am I to configure P1.2 and P1.3 as analog or digital?....Seems that I would be prohibited from using the SEEED connection in analog and I2C (P1.2 / P1.3) at the same time if I cannot ONLY configure A1 and A4 as analog