This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR6047: MSP430FR6047 programing using UART BSL+ Rocket + BSL-scripter

Part Number: MSP430FR6047


trying to load .txt file using BSL + Rocket + BSL-scripter

getting following error,

I am unable to understand the problem, please suggest

Attached are script file and .txt file

 153C07A0W.txt

//
//Script example FRxx UART BSL
//
//Device : MSP430FR6989
//Comm Bridge: MSP-BSL Rocket
//
//Download blink application through
//UART BSL in FRAM device
//
LOG
MODE FRxx UART 9600 COM14
//gives wrong password to do mass erase
RX_PASSWORD pass32_wrong.txt
//
//add delay after giving wrong password
//because the device does not give
//any response after wrong password applied
//
DELAY 2000
RX_PASSWORD pass32_default.txt
RX_DATA_BLOCK 153C07A0W.txt
//CRC_CHECK 0x4400 0x0020
//SET_PC 0x4400
pause

**Attention** This is a public forum