Part Number: MSP430F2274-EP
I am working on a BLDC controller using this extended-temperature MSP430 part. Almost all of this design is adapted from a similar design that used a C2000 DSP as the controller, we swapped in the MSP430 because a different application required a low-power state.
We are now doing environmental tests on the controller and we are getting some odd behavior at ambient temperatures above about 92C*. It appears that an incorrectly high value is being read at the ADC10 for our current sensor. There is nothing in that signal path that is different from the previous design (which works correctly at these temperatures) other than the microcontroller.
Is there a known issue with ADC offset at high temperatures in the MSP430?