Part Number: MSP430FR5994
Dear Sir,
We are using MSP430FR5994. When I kept turning on the power of MSP430FR5994 continuously, there was a problem that the internal clock stopped in about 3 to 4 days. I decided that the internal clock was stopped because I confirmed that the timer interrupt did not work even though the PWM continued to output. Have you ever experienced a similar phenomenon? Also, please let me know if you have any countermeasures. Currently, I think that EMC has an effect on the SBWTDIO terminal and that is the behavior. Also, the frequency of occurrence is not 100%, but 30% of the boards. It has been discovered as a mass-produced product by pre-shipment inspection. We are in urgent need of help, so please cooperate.