Other Parts Discussed in Thread: MSP430F2272, MSP-FET
I have a MSP-FET Flash Emulation Tool and I want to load a firmware into MSP430F2272 microcontrolle via command line interface.
I have two emulators, one is MSP-FET430UIF (white-grey) and other is MSP-FET Flash Emulation Tool (black) I am using MSPFlasher tool with MSP-FET Flash Emulation Tool and I receive the next message:
Accessing device...
Exit:16
ERROR: Unknown device
With MSP-FET430UIF emulator the output is:
Setting VCC to 3000 mV...
Exit:44
ERROR: Could not set device Vcc
I use TDI signal to communicate with MSP430F2272 micro, I mean, Spy Bi Wire communication.
Any idea about the problem?