Part Number: MSP430FR6043
Hi!
My environment:
CCS: 10.1
MSP SDK: 3.80.10.09
CC SDK: 4.30.00.54
Devices:
MSP430FR6043
Launchpad CC1352R1 rev. B
Problem:
I created example project from UltrasonicWaterFR604x_02_40_00_00. I want to connect CC to MSP with SPI, where MSP working as a slave. I added my SPI driver implementation in comm/drivers/ and another option in comm_config.h (COMM_SPISLAVE).
I configured SPI on EUSCI_A_SPI with P4.2, P4.1, P4.3 and P4.4 pins. Also I added two GPIO pins for handshake (P3.1 and P4.0). At this moment everything seems to work fine, GPIO handshake is working and I have interrupt on P3.1, but SPI interrupt is never invoked.
Setup on MSP:
// Params:
param.msbFirst = EUSCI_A_SPI_MSB_FIRST;
param.clockPhase = EUSCI_A_SPI_PHASE_DATA_CAPTURED_ONFIRST_CHANGED_ON_NEXT;
param.clockPolarity = EUSCI_A_SPI_CLOCKPOLARITY_INACTIVITY_LOW;
param.spiMode = EUSCI_A_SPI_4PIN_UCxSTE_ACTIVE_LOW;
EUSCI_A_SPI_select4PinFunctionality(EUSCI_A0_BASE, EUSCI_A_SPI_ENABLE_SIGNAL_FOR_4WIRE_SLAVE);
EUSCI_A_SPI_enable(EUSCI_A0_BASE);
EUSCI_A_SPI_clearInterrupt(EUSCI_A0_BASE, EUSCI_A_SPI_RECEIVE_INTERRUPT);
EUSCI_A_SPI_enableInterrupt(EUSCI_A0_BASE, EUSCI_A_SPI_RECEIVE_INTERRUPT);
// and Interrupt:
#pragma vector=USCI_A0_VECTOR
__interrupt void USCI_A0_ISR(void) { ... }
Setup on CC:
params.transferMode = SPI_MODE_CALLBACK; params.frameFormat = SPI_FrameFormat::SPI_POL0_PHA0; params.bitRate = 10000; params.mode = SPI_Mode::SPI_MASTER; params.dataSize = 8;
I start transfer from CC side, and working like a charm with example spi project from MSP SDK (eusci_a_spi_ex1_slave), but in UltrasonicWaterFR604x_02_40_00_00 example project it's never reach SPI interrupt.
How can I fix it?