This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR6043: SPI with Low Power Mode.

Part Number: MSP430FR6043

My environment:

CCS: 10.1
MSP SDK: 3.80.10.09
CC SDK: 4.30.00.54


Devices:

MSP430FR6043
Launchpad CC1352R1 rev. B

Problem:

Hi!

I have single configuration: MSP connected to CC with SPI, where CC is in master mode and MSP in slave. In normal life they communicate within 1 to 10 seconds. Now MSP once per 3s wants to transmit data to CC, but also I want MSP to save as much energy as possible.

I wonder when and how can I go LPM with MSP, i.e. can I go LPM4 and still have SPI open with interrupt registered? Or should I close SPI every time when I want go LPM and wake up processor with GPIO interrupt?

How can I (or how should I?) combine SPI with LPM?

**Attention** This is a public forum