Part Number: MSP430F67791A
I am using the MSP430f67791a as an analog front end for metering. The MSP drives an SPI output with 10MHz clock to a larger Linux processor. What is a best approach to get the MSP430 on an Ethernet LAN for comms to the larger processor? This is not a routing situation - straight Ethernet could be used on the cable. There would be multiple (up to 10) MSP430s on the LAN streaming to one larger processor. Currently there is no OpSys on the MSP430.